TIDUF15 March 2023
The TIVA MCU debug interface has a USB-to-I2C interface. The Application Customization Tool can be used to interface the TPS65994 using the Read/Write registers via TIVA MCU. J10 is an Aardvark™ interface which can optionally be used with the third party USB-to-I2C interface hardware box. Additionally, the U11 switch is used to enable the MCU or Aardvark interface to write to the DC/DC converter or the USB-C redriver by accessing either the PD controller or via I2C3 communication.