TIDUF18A October 2022 – February 2024
The totem-pole PFC operates in the positive and negative cycles of the AC mains input, respectively, and determines the current flow depending on how the high frequency GaN MOSFETs are switched (see Figure 3-2 and Figure 3-3, respectively).
The high-frequency GaN MOSFETs together with the inductor create a synchronous mode boost converter. During the positive half cycle, S2 is the boost switch which is driven with duty cycle D and S1 is driven with a complementary pulse-width modulation (PWM) signal (1-D). Figure 3-2 (A) shows the direction in which the current flows. Similarly, during the period when S2 is switched with 1-D, S1 is switched with D; Figure 3-2 (B) shows the direction in which the current flows. Note that, during this cycle, SD2 conducts continuously.
During the negative half cycle, the operation is similar except that the role of the high-side- and low-side, high-frequency switches are swapped. Figure 3-3 shows the direction in which the current flows. Note that, during this cycle, SD1 conducts continuously.
This reference design uses GaN FETs (LMG3522R030-Q1) and TI’s C2000™ Piccolo™ (TMS320F280039C) high-performance MCU. The high-frequency GaN FETs operate at a 120-kHz switching frequency and the pair of Si MOSFETs operate at the line frequency (approximately 45 Hz to 60 Hz). Thus the conduction path includes one GaN switch and one low-frequency Si switch with significantly-reduced conduction losses. The use of two-channel interleaving to reduce conduction loss and input current ripple. Test results demonstrate a high efficiency above 98.5%.