TIDUF23 may 2023
If not installed, download and install Code Composer Studio (CCS) which is needed to build and run the project. CCS version 12.2.0 or newer is recommended for this project. CCS User's Guide provides more details about CCS installation and use.
The software for TIDM-02014 is provided as part of C2000Ware MotorControl SDK. Note that C2000Ware MotorControl SDK installation is separate from CCS installation. Once the SDK is installed, use the following guidelines to import and run the project in CCS.