TIDUF25 june 2023 ADS131M08 , MSPM0G1507
The software for displaying the metrology parameters on the LCD is not implemented yet. For each metering parameter that gets displayed on the LCD, three items are usually required: (1) a symbol used to denote the phase of the parameter, (2) text to denote which parameter is being displayed, and (3) the actual value of the parameter. The phase symbol is displayed at the top of the LCD and denoted by a triangle shape. The orientation of the symbol determines the corresponding phase.
If running, the LCD typically scrolls between metering parameters every two seconds.