TIDUF25 june 2023 ADS131M08 , MSPM0G1507
For the following test results, gain and phase calibration are applied to the meter. In the following results, the active energy results are within 0.1% at 0° phase shift. Additionally, the active energy versus voltage results and the RMS voltage results show that good accuracy results are able to be obtained despite using only a fraction of the ADC range for the voltage channels.
The "% Error" columns in the following 6 tables and plots are calculated as the difference between the multiple reference input values to TIDA-010243 and the measured values, shown on the PC GUI. The reference input values to TIDA-010243 are generated by a PTS3.3C Source Generator/Reference Meter from the company MTE, while the measured values calculated by the TIDA-010243 Energy Library are reported in the PC GUI.
VOLTAGE (V) | % ERROR |
---|---|
270 | 0.00555 |
260 | 0.00384 |
240 | 0.00375 |
230 | 0.01086 |
220 | 0.00863 |
200 | 0.00700 |
180 | 0.01055 |
160 | 0.00250 |
140 | 0.00214 |
120 | 0.00666 |
100 | 0.00300 |
90 | 0.01300 |
70 | 0.01571 |
50 | 0.00240 |
30 | 0.01200 |
10 | 0.00299 |
9 | 0.02733 |
CURRENT (A) | % ERROR |
---|---|
0.01 | 0.50383 |
0.03 | 0.20413 |
0.05 | 0.07749 |
0.1 | 0.00399 |
0.25 | 0.02239 |
0.50 | 0.00179 |
1.00 | 0.01999 |
2.00 | 0.01649 |
5.00 | 0.00539 |
10.00 | 0.00999 |
20.00 | 0.01449 |
30.00 | 0.03366 |
40.00 | 0.01124 |
50.00 | 0.01398 |
60.00 | 0.01566 |
70.00 | 0.00642 |
80.00 | 0.00749 |
90.00 | 0.02321 |
100.00 | 0.02099 |
VOLTAGE (V) | % ERROR |
---|---|
270 | 0.01444 |
260 | 0.01307 |
240 | 0.00500 |
230 | 0.00304 |
220 | 0.01090 |
200 | 0.00500 |
180 | 0.00111 |
160 | 0.00687 |
140 | 0.00428 |
120 | 0.01916 |
100 | 0.00900 |
90 | 0.00922 |
70 | 0.02771 |
50 | 0.02240 |
30 | 0.02500 |
10 | 0.03400 |
9 | 0.02133 |
CURRENT (A) | % ERROR |
---|---|
0.01 |
0.63311 |
0.03 |
0.26816 |
0.05 |
0.07893 |
0.10 |
0.04498 |
0.25 |
0.01159 |
0.50 | 0.01220 |
1.00 | 0.01499 |
2.00 |
0.00449 |
5.00 | 0.01339 |
10.00 |
0.00100 |
20.00 |
0.01449 |
30.00 | 0.02666 |
40.00 |
0.02825 |
50.00 |
0.01019 |
60.00 | 0.01683 |
70.00 | 0.00414 |
80.00. | 0.00475 |
90.00 | 0.01988 |
100.00 | 0.03199 |
VOLTAGE (V) | % ERROR |
---|---|
9 | 0.02077 |
10 | 0.00699 |
30 | 0.00566 |
50 | 0.00960 |
70 | 0.00528 |
90 | 0.00988 |
100 | 0.00200 |
120 | 0.00999 |
140 | 0.00071 |
160 | 0.01874 |
180 | 0.00388 |
200 | 0.00650 |
220 | 0.00090 |
230 | 0.01652 |
240. | 0.01124 |
260 | 0.02461 |
270 | 0.02444 |
CURRENT (A) | % ERROR |
---|---|
0.01 | 0.32617 |
0.03 | 0.15916 |
0.05 | 0.09126 |
0.10 | 0.00499 |
0.25 | 0.00200 |
0.50 | 0.01940 |
1.00 | 0.00500 |
2.00 | 0.00699 |
5.00 | 0.01139 |
10.00 | 0.09506 |
20.00 | 0.05700 |
30.00 | 0.02899 |
40.00 | 0.03625 |
50.00 | 0.01720 |
60.00 | 0.01166 |
70.00 | 0.01842 |
80.00. | 0.01062 |
90.00 | 0.00100 |
100.00 | 0.00120 |