TIDUF28 November 2023
The power losses of the 1-mΩ shunt at nominal maximum output current of 7.7 ARMS without heat sink are 60 mW with a capability to handle 40 ARMS (transient) at 1.6-W losses in the case where a heat sink is mounted with that design. The package and power rating of the shunt R16 were chosen for 3 W to also have an option to be replaced with higher resistance shunts, such as 5 mΩ to evaluate the AMC1306M25 with ±250-mV linear input voltage range and test the system at higher load current with a heat sink for the bottom-side cooled GaN-FETs.
In the layout, use a Kelvin connection from the shunt to the differential input filter R26, R29, C40 and route the signal AIN_N and AIN_P differentially. Connect the AMC1306 AGND to the shunt terminal which is connected to the top-side source (SW) of the GaN-FET. For easier routing in this design, AIN_N has the same potential as switch node (SW) and the phase current measures the inverted motor phase current.