Use the following steps to run the code for Lab 1.
- Use the test setup shown in Section 3.3.1.
- Run the project by clicking
from the menu bar. - In the watch view, check if the
BT2PH_InputVoltageSense_V is between 12V -15V in the Expression
Window.
- Check DRDY signal of the external ADC if
the frequency is 15.625 kHz using an oscilloscope. Figure 3-25 shows the DRDY and CS signal of ADS131M08 when the MCU is running.
- Set the following parameters from the
Expression Window:
- BT2PH_userParam_V_I_ch1->dutyRef_pu = 0.03
- Set the
BT2PH_userParam_V_I_ch1->en_bool = 1
- Set the
"BT2PH_enableRelay_bool" to 1 to enable the output relay
- See Figure 3-13 for the Expression Window settings
- BT2PH_measureMultiphase_V_I variable shows output
current and voltage of the DC/DC converter. Adjust the
BT2PH_userParam_V_I_ch1->dutyRef_pu to make sure the current is approximately
15 A.
- SFRA Setup for Open-Loop
Current ControlSFRA Setup for Closed-Loop
Current ControlSFRA Setup for Open-Loop
Voltage ControlSFRA Setup for Closed-Loop
Voltage Control shows the SFRA setup to extract the plant model for Open-Loop Current
Control. Click on the Run SFRA icon from the SYSCONFIG page. The SFRA GUI
pops up.
- Select the options for the device on the SFRA
GUI; for example, for F280039, select floating point. Click on Setup
Connection. In the pop-up window, uncheck the boot-on-connect option and
select an appropriate COM port. Click the Ok button. Return to the SFRA GUI and
click the Connect button.
- The SFRA GUI connects to the device. An SFRA
sweep can now be started by clicking Start Sweep. The complete SFRA sweep
takes a few minutes to finish. Once complete, a graph with the measurement
appears, as shown in Figure 3-15.
- The Frequency Response Data is saved in the
project folder, under an SFRA Data Folder, and is time-stamped with the time of
the SFRA run.