TIDUF35 june 2023 AM6442
The DP83TD510E is an ultra-low power Ethernet physical layer transceiver compliant with the IEEE 802.3cg 10Base-T1L specification. The PHY has very-low-noise coupled receiver architecture enabling long cable reach and very-low power dissipation. The PHY supports a long cable reach of more than 2000 meters. The DP83TD510E has external MDI termination to support intrinsic safety requirements. The device interfaces with the MAC layer through MII, Reduced MII (RMII) , RGMII, and RMII low-power 5-MHz master mode. This reference design used the RGMII interface for the connection between MAC and PHY.