TIDUF43 August 2024
For this test, an ammeter was connected in series at the VBAT input to measure the current in low power mode. No load is connected at the output. Figure 4-5 corresponds to the system IQ without an MCU, and Figure 4-6 corresponds to the system IQ with an MCU.