TIDUF43 August 2024
Figure 3-4 shows a state machine that best describes the TIDA-020065. Initially, the MCU boots up and enters precharge mode to charge the load capacitors for 15ms. After this 15ms period has expired, the system transitions over to active mode by pulling nLPM high.
In active state, the main FET is being driven for loads up to 30A. S3 can be pressed to transition the system from active to low power mode. S2 can also be used to switch between the programmed time-current fuse characteristics.
The ADC peripheral of the MSPM01306 collects samples every 100μs to constantly monitor the output current in active mode. When an overload current is detected, the system promptly transitions from active to shutdown mode. Depending on how long the current pulse is active, and how high the pulse is, the software uses the programmed time-current characteristics to protect the wire harnesses and load for the current ranges shown in Figure 3-5.
The software I2t algorithm replicates the behavior of an actual melting fuse; the output is shutdown before peak load transients or other overcurrents cross the wire current capability and damage the vehicle wiring. The I2t algorithm is best explained by Equation 10.
where
To better simulate a real
fuse, is subtracted from the
measurement every time an ADC sample is
taken. This addition allows the smart fuse to operate at the Inom threshold and to
avoid falsely shutting down due to normal load transients.
To bypass limitations with only being able to run the I2t algorithm up to the maximum monitorable current, which is 66A in this design, a fixed-delay shutdown threshold was added to shutdown the output at a fixed time up until the SC threshold. Although 4ms was chosen for the fixed-delay shutdown time for this design, set this time according to what current pulses are allowed in the system.
When either fuse shutdown or fixed-delay shutdown occurs, the system transitions over to cooldown mode, where INP is pulled low and the system is allowed to recover from the overload event. By default, the MSPM0L1306-Q1 automatically pulls INP high again in 4s to recover the output. Nonetheless, the software can be configured by pulling TP14 low for latch-off behavior in cooldown mode. The output now stays off indefinitely until user input is received by pressing either S2 or S3. Comparing this behavior to a melting fuse shows that melting fuses have to be replaced whereas this design allows for resettable overcurrent protection. In a more realistic application, the software considers the thermals of the vehicle wiring to make sure that enough time has elapsed to cool the wire harnesses down.
For immediate shutdown, the short-circuit protection feature of the TPS1213-Q1 is used. nFLT is pulled low to signal to the MSPM0L1306-Q1 that a hardware fault was detected. In this state, pressing S2 or S3 toggles INP which clears the SC protection latch of the TPS1213-Q1.