TIDUF44 January 2024
In the main current loop, this design places a D12 voltage regulator tube at the PACK interface, and the parameters of the voltage regulator tube can be selected according to the number of strings in the system. In addition, the design also places a diode D13, which can provide a clamp after the PACK terminal is short-circuited. C29 and C31 (ESD capacitors which are designed to change the direction of ESD current) were also added. There are two for redundancy purposes in case one of them gets damaged or shorted.