TIDUF45 May 2024
Use the basic setup in Figure 4-3 to evaluate the PCB. The board is evaluated through the PHI board to a PCB running the ADS127L21EVM-PDK-GUI software. The default reference value in the GUI is 2.5V, which must be updated to 4.096V.
The following components are required to run all tests:
Connect the hardware and power on as shown in Figure 4-3.
Use twisted pairs or SMA connectors to connect the precision DC source to the input of the signal chain, using the shortest connections possible. This reduces the amount of noise coupled into the signal chain, allowing for high-accuracy measurements.
To test a single-ended signal, connect the negative input (AINN) directly to ground using jumper J17 and connect the desired signal to the positive input (AINP) using the SMA connector (J19) or one of the pin connectors (J18 pin 2, or J20 pin 1).