TIDUF46 October 2023
Figure 2-2 shows the strategy of reading all thermistors and cell voltages. Two TMUX1308 devices are used to multiplex 16 Negative Temperature Coefficient (NTC) thermistors to one BQ79616. The BQ79616 uses three GPIOs (GPIO5, GPIO6, and GPIO7) to address the 8 NTC thermistor channels of the TMUX1308 and two GPIOs (GPIO1 and GPIO2) to read the common output pin from two TMUX1308 devices. This means 5 GPIOs can switch 16 NTC thermistors. If more thermistors are required, 6 GPIOs can switch 24 NTC thermistors.
Although the number of NTC thermistors can easily be increased using the TMUX1308 or a different multiplexer, the system still needs an efficient switching strategy to connect all 16 NTC thermistors in a safe time defined by regulation.
The loop of NTC thermistor switching consists of a broadcast write to all the stacked BQ79616 GPIO5 to 7 pins and a broadcast read of the TSREF and GPIO1 to GPIO2. The design needs 8 loops to read the temperature data from 16 NTC thermistors. Supposing the number of stacked BMUs is N, and the design uses a BQ79600 base device (not counted when determining N), then one loop spends to perform the broadcast write to the GPIO5 to7 pins on all devices. A broadcast read of the TSREF and GPIO1 to GPIO2 takes
If the BESS rack voltage is 1500 V, and one rack consists of 470 pieces of battery cells in series, then use 15 BMUs (30 BQ79616 devices) to monitor all the battery cells. Performing one loop to read temperature data from the stacked BQ79616 devices takes 4.11 ms and polls 2 out of the 16 NTC thermistors on each BQ79616 in the stack. Reading temperature data from all 16 NTC thermistors on each BQ79616 in the stack takes 32.880 ms. Following the NTC thermistors data reading, 11.706 ms are required to read the cell voltage (VCELL) data of all the stacked BQ79616 devices. The total time spent gathering temperature and VCELL data for a 1500-V rack is about 44 ms, which meets GBT34131-2023 standards (100 ms for VCELL and 1 s for NTC thermistors).