TIDUF56 January 2024
This section describes the procedure to run the setup using the software provided with the design. The designer must have previously set up the hardware and software as described in Section 4.2.
However, if the motor type and the test parameters need to be changed, the parameters are found in the settings.h file. The default settings can be changed by changing the value of the USER_MOTOR macro. If you intend to use a motor outside the list of predefined motors, copy the template used.