TIDUF57 November 2023
The current-sense resistor RCS is determined after initially calculating a value for a traditional current-sense resistor, RCS(trad). An initial value for RCS(trad) can be selected with considerations for the feedback voltage and other gain factors in the feedback loop as explained by Equation 14:
where
RCS is then determined by solving for the traditional current-sense design resistance, RCS(trad), and multiplying by the inverse of GCSE, the current sense gain, equal to 1,036 mA/A. The traditional current-sense design creates the current-sense voltage, VCS(trad), by passing the GaN power FET drain current, ID, through RCS(trad). The LMG3624 creates the current-sense voltage, VCS, by passing the CS pin output current, ICS, through RCS. The current-sense voltage must be the same for both designs.