TIDUF57 November 2023
The quasi-resonant converter is chosen because this converter provides the best balance between cost, power loss, and simplicity.
The converter consists of a diode rectifier stage, switching FET, transformer with an inherent magnetizing inductance, passive RC clamp, synchronous secondary rectifier, and output capacitor.
The diode rectifier stage consists of the diode bridge and bulk capacitor. The diode bridge rectifies the ac line voltage and stores energy in the bulk capacitor, which maintains a relatively constant positive voltage.
The controller switches the FET on and off to deliver energy to the secondary side. While the FET is in the on state, current (energy) is built up in the magnetizing inductance of the transformer.
This is described by Equation 1:
The power delivered is calculated with Equation 2:
While the FET is in the off state, the rectifier on the secondary side of the transformer turns on and delivers the current to the load.
To maximize efficiency, the converter operates under quasi-resonant operation by turning on the FET at the resonant voltage valley formed by the resonance of the magnetizing inductance,LMAG, and the total switch-node capacitance,CD.
At this voltage valley, the FET suffers from the lowest possible turn-on switching power loss as described using Equation 3:
where
The minimum valley at which the converter can switch is given with Equation 4:
Equation 4 illustrates that the VVALLEY,MIN reaches zero volts when the rectified input voltage, VIN,DC, is equal to or less than the reflected voltage, NPS × VOUT. Hence, the quasi-resonant converter operates with zero-voltage switching under conditions when the input voltage is low and the reflected voltage is high, meaning that device losses are only conduction-dominated.