TIDUF58 June 2024
Low ripple and low noise normally indicate two different features of power supply. Ripple refers to the output voltage variation with switching frequency, which is measured by scope and reduced by using second stage LC filter. Noise normally refers to the voltage variation in frequency range of 100Hz-100kHz, which is usually measured with noise spectrum and limited by unique IC design. For some application which only requires low ripple but not low noise, a second stage LC filter design method is proposed for general purpose peak current mode buck regulators.
Figure 2-2 shows the scheme of buck converter with second stage filter. A second-order low pass filter is formed by inductor L2 and capacitor C2. A new pair of conjugate poles is introduced with the filter, which can reduce the output voltage ripple and noise at switching frequency through the high frequency gain attenuation. The selection method of inductor L2 and capacitor C2 are analyzed in the application note.
Figure 2-3 to Figure 2-5 show the schemes of power designs with second stage filter, correspond to the power designs with first stage sense, second stage sense and hybrid sense. The following summarizes advantages and disadvantages of each design.
Due to the obvious advantages of hybrid sense, the reference design is based on this sense approach.
Figure 2-6 shows the TIDA-050073 Block Diagram, using a PCM buck converter TPS62933F with second stage filter and hybrid sense. The application note discusses how to analyze hybrid sense loop stability.