To start CCS and open the project, complete the following steps:
- Connect a programmable, isolated AC source
capable of providing universal AC input up to 750 W to the input terminals
(connector J5) of the reference board as shown in Figure 3-29. Set the AC source current limit to 8 A. Do not turn the
power supply on at this time.
- Connect a motor (compressor) to J10.
- Follow Steps 2 and 3 of Section 3.3.4.1.1 to open the project.