TIDUF60 December 2023
Two techniques are supported to measure phase currents of the motor.
Either one of these two current sensing techniques can be selected in the build configuration of the project. The Flash_MtrInv_3SC build configuration supports three-shunt current sensing method, the Flash_MtrInv_1SC supports single-shunt current sensing method as described in Section 3.3.2.