TIDUF60 December 2023
The 3-phase voltages, currents, and fluxes of AC motors can be analyzed in terms of complex space vectors. With regard to the currents, the space vector can be defined as follows. Assuming that ia, ib, ic are the instantaneous currents in the stator phases, then the complex stator current vector is defined in Equation 6.
where
Figure 2-9 shows the stator current complex space vector.
where
This current space vector depicts the three-phase sinusoidal system which still needs to be transformed into a two time invariant co-ordinate system. This transformation can be split into two steps: