TIDUF60 December 2023
On the Debug Window tab, the PI regulators can be tuned for speed, current, and power control as shown in Figure 3-14. The values are coefficient, the final gains are that these coefficients multiply the setting value in the C2000 controller. The setting gains are calculated per the motor electrical parameters. As Figure 3-9 shows, those tuned values can be written to MCU flash.