TIDUF60 December 2023
The space vector can be reported in another reference frame with only two orthogonal axis called (α, β). Assuming that the axis a and the axis αlpha are in the same direction yields the vector diagram shown in Figure 2-10.
The projection that modifies the 3-phase system into the (α, β) 2-dimension orthogonal system is presented in Equation 7.
The two phase (α, β) currents are still dependent on time and speed.