TIDUF60 December 2023
As explained in Section 2.4.1.7, the internal CMPSS can be configured for overcurrent protection. Figure 3-42 shows the internal overcurrent protection waveform, is triggered by internal CMPSS, since both IPM_FALUT and IPM_CIN are not triggered. Overcurrent can be set with the following codes.
objSets->maxPeakCurrent_A = USER_M1_ADC_FULL_SCALE_CURRENT_A * 0.4975f;