TIDUF60 December 2023
Figure 2-20 shows the conventional PLL integrated into the SMO.
The traditional reduced-order sliding-mode observer is constructed, with the mathematical model shown in Equation 14 and the block diagram shown in Figure 2-21.
where
where
If and are positive and significant enough to provide the stable operation of the SMO, then and are large enough to hold and .
The estimated value of EEMF in α-β axes ( , ) can be obtained by low-pass filter from the discontinuous switching signals and :
where
Therefore, the rotor position can be directly calculated from arc-tangent the back EMF, as Equation 17 defines:
Low-pass filters remove the high-frequency term of the sliding-mode function, which results in phase delay. The delay can be compensated by the relationship between the cut-off frequency and back EMF frequency , which is defined as shown in Equation 18:
Then the estimated rotor position by using SMO method is found with Equation 19:
In a digital control application, a time-discrete equation of the SMO is needed. The Euler method is the appropriate way to transform to a time-discrete observer. The time-discrete system matrix of Equation 14 in α-β coordinates is given by Equation 20 as:
where
The time-discrete form of Equation 16 is given by Equation 23 as: