TIDUF61 May 2024
Figure 3-10 shows the TIDA-020069 board configured in the short-to-ground failure state. In this state, the HVIL load has experienced a short to ground at some point in the loop. This short can occur before, after, or between the load resistors. This replicates the failure mode within an HEV/EV, as the HVIL system cannot determine if the connectors are in a closed or open configuration during this short failure.
The Short to Ground LED indicator is turned on in Figure 3-10, as expected for this state. This verifies the logical interpretation of the HVIL-Send and HVIL-Return voltages in this state.