TIDUF61 May 2024
Figure 3-8 shows the TIDA-020069 board configured in the open connection state. In this state, the HVIL load resistors are disconnected at some point within the HVIL loop and no current is flowing through the load. This replicates the a scenario within an HEV/EV where a high-voltage connector is disconnected. An open connection can be experienced during vehicle maintenance or as a result of collision. In this state, the high-voltage connectors are not connected and the HVIL loop is view as an open connection.
The Open Connection LED indicator is turned on in Figure 3-8, as expected for this state. This verifies the logical interpretation of the HVIL-Send and HVIL-Return voltages in this state.