TIDUF63A December 2023 – June 2024
Transformers for resonant converters need to be designed to have enough magnetizing current to discharge output capacitance of the switches on both the sides. There are two conditions to be met. Make the energy stored in magnetizing and resonant inductors bigger than energy stored in output capacitance of switches on both sides. Also, the magnetizing current needs to be big enough to discharge capacitance of switches within a given dead time.
where
where
The first condition (Equation 4) is the energy requirement and the second condition (Equation 5) is the slew rate requirement.
The peak magnetizing current is a half of the peak-to-peak value of magnetizing current.
The equivalent capacitance is the sum of capacitance on the LV side plus capacitance of the HV side reflected to the LV side:
where
The reflected capacitance C'S can be calculated using transformer ratio:
where
The output capacitance of switches limit the maximum magnetizing inductance. Select switches as a trade-off between RDS(on) and COSS.