TIDUF64A December 2023 – August 2024
Voltage sensing provision is provided at two points in the inverter signal path to aid in control: before and after the output relay. By enabling measurement on both sides of the relay, the control system can lock into the grid voltage and frequency before connecting, thus preventing any mismatch issues. OPA2388 is used a which is a dual channel operational amplifier. Both the channels are used for the AC voltage measurements. The DC bus voltage is also sensed using another OPA2388 .