TIDUF64A December 2023 – August 2024
In any power converter design, the inductor design is the most important part. The four important characteristics pertaining to the inductor design are namely the inductance value, ripple current, saturation current and the DC resistance (DCR).
Normally, the value of inductance can be calculated with Equation 7
where,
Hence, the inductor ripple can also be given by Equation 8
where,
The worst-case duty cycle for a boost converter or a single-phase converter is can be seen from Figure 1-3, to be at 25%. Hence the inductance value is calculated for the corresponding condition. Normally, it is advisable to work with an inductor peak-to-peak current of less than 40% of the average inductor current for maximum output current. A smaller ripple from a larger valued inductor reduces the magnetic hysteresis losses in the inductor and EMI. The saturation current of the inductor must be higher than the calculated peak inductor current.
In a boost regulator, the inductor DC current can be calculated by Equation 9
where,
Therefore, the inductor peak current is calculated with Equation 14,
where,
iL(pk-pk) is the peak-to-peak inductor current ripple