TIDUF67 April 2024 – December 2024
The conventional PLL integrated into the SMO is shown in Figure 3-8.
The traditional reduced-order sliding mode observer is constructed, which mathematical model is shown in Equation 13 and the block diagram is shown in Figure 3-9.
where zα and zβ are sliding mode feedback components and are defined as:
Where kα and kβ are the constant sliding mode gain designed by Lyapunov stability analysis. If kα and kβ are positive and significant enough to maintain the stable operation of the SMO, the kα and kβ are usually large enough to hold Equation 15 and Equation 16.
The estimated value of EEMF in α-β axes (Equation 18, Equation 19) can be obtained by low-pass filter from the discontinuous switching signals zα and zβ:
Where Equation 20 is the cutoff angular frequency of the LPF, which is usually selected according to the fundamental frequency of the stator current.
Therefore, the rotor position can be directly calculated from arc-tangent the back EMF, defined as follows
Low pass filter removes the high-frequency term of the sliding mode function, which leads to occur phase delay resulting. This can be compensated by the relationship between the cut-off frequency ωc and back EMF frequency ωe, which is defined as:
And then the estimated rotor position by using SMO method is:
In a digital control application, a time discrete equation of the SMO is needed. The Euler method is the appropriate way to transform to a time discrete observer. The time discrete system matrix of Equation 13 in α-β coordinates is given by Equation 24 as:
Where the matrix [F] and [G] are given by Equation 25 and Equation 26 as:
The time discrete form of Equation 17 is given by Equation 27 as: