The system is gradually tested and
verified in multiple stages so that the final system can be confidently operated. To select a
particular build option, change the value of the DMC_BUILDLEVEL define to the desired
DMC_LEVEL_X option in the sys_settings.h file. After the build option is selected,
compile the project by right-clicking on the project name and clicking Rebuild
Project.