TIDUF67 April 2024
TMDSHVMTRINSPIN is a DIMM100 controlCARD based motherboard evaluation module showcasing control of the most common types of high voltage, three-phase motors including AC induction (ACI), brushless DC (BLDC), and permanent magnet synchronous motors (PMSM). The High Voltage Motor Control Kit has individual DC bus and three-phase voltage sensing making this board for BLDC/PMSM control with TI controlCARD™ an excellent choice for use with the sensorless FOC algorithm.
This section explains the steps needed to run the TMDSHVMTRINSPIN with the software supplied through MotorControl SDK. The kit ships with the jumper and switch settings correctly positioned for connecting with the controlCARD. Make sure that these settings are valid on the board as described in the following, and then insert the controlCARD with the TMDSADAP180TO100 adapter into the TMDSHVMTRINSPIN board as shown in Figure 4-10.
Table 4-6 shows the various connections available on the board. The location of these connections on the board are shown in Figure 4-11.
[Main]-P1 | AC input connector (110V – 220VAC) |
[Main]-TB3 | Terminal Block to connect motor |
[Main]-BS1 | Banana Jack for Output from AC Rectifier |
[Main]-BS2, BS6 | Banana Jack for GND Connection |
[Main]-BS3 | Banana Jack for connecting an input voltage for the PFC stage, this is typically rectified AC voltage from the [Main]-BS1 connector. |
[Main]-BS4 | Banana Jack for connecting a load to the output from the PFC stage, When using PFC+Motor project the output of the PFC stage is connected to the input for the inverter bus for example [Main]-BS5 |
[Main]-BS5 | Banana Jack for input of DC bus voltage for the inverter |
[Main]-J2 | Aux power supply module input voltage
selection jumper,
|
[Main]-J3, J4, J5 | Jumpers J3,J4 and J5 are used for sourcing 15V, 5V and 3.3V power respectively for the board from the 15V DC Power supply. |
[Main]-J7 | J7 is used to select the over current protection threshold source |
[Main]-J8 | J8 is used to enable/disable the IPM over current protection |
[Main]-J9 | JTAG TRSTn disconnect jumper, populating the jumper enables JTAG connection to the Microcontroller. The jumpers need to be unpopulated when no JTAG connection is required such as when booting from FLASH. |
[Main]-J14 | PWMDAC outputs: Gives voltage outputs that result from a PWM being attached to a first-order low-pass filter. Pins 1,2,3 and 4 are attached to low pass filtered PWM output pins respectively to observe system variables on an oscilloscope. |
[Main]-J16 | Isolated CAN bus connector |
[Main]-J17 | Connector to supply power to the DC fan (shipped with the board) that is attached to the IPM heat sink. |
[Main]-H1 | QEP connector: connects with a 0-5V
QEP sensor to gather information on a motor’s speed and position. CAP/Hall effect sensor connector: connects with a 0-5V sensor to gather information on a motor’s speed and position. |
[M1]-F1 | Fuse for the AC input |
[M3]-JP1 | USB connection for on-board emulation |
[M3]-J2 | External JTAG interface: this connector gives access to the JTAG emulation pins. If external emulation is desired, place a jumper across [M3]-J5 and connect the emulator to the board. To power the emulation logic a USB connector still needs to be connected to [M3]-JP1. |
[M3]-J5 | On-board emulation disable jumper: Place a jumper here to disable the on-board emulator and give access to the external interface. |