Download and install MOTOR-CONTROL-SDK-AM263X software package from the link provided by TI, install
this Motor Control SDK software in the default folder. MOTOR-CONTROL-SDK-AM263X can be installed in one of two ways:
Go to CCS and under View → Resource
Explorer. Under the TI Resource Explorer, go to Arm®-based microcontrollers → MOTOR
CONTROL SDK for AM263x, and click on the install button.
Once the installation is complete, close
CCS, and create a new workspace for importing the project. Follow the steps to build and
run this project with different incremental builds as described in the following
sections.