TIDUF67 April 2024 – December 2024
AM263_xxx.syscfg file configures the function of the GPIO pins and sets the direction and mode of the specified pin according to the hardware motor driver board/kit that is used. For modifying the code for a custom board, a TI motor driver EVM that does not currently have universal lab code support, or for use with a different TI MCU, these GPIO assignments need to be changed to correspond properly with the motor driver board.