TIDUF68 February 2024
To see the effective parasitic capacitive losses, the TIDA-010936 PCB power losses were measured at zero load current with 50% PWM duty cycle and PWM switching frequencies from 8kHz to 80kHz, as shown in Equation 3.
The simulation was done using COSS(TR) = 501pF from the LMG2100R044 data sheet, while adding an additional 80pF equivalent board related capacitance due to PCB and cabling parasitic capacitances.
To subtract the supply current offset on the TIDA-010936 at zero PWM switching, a first measurement was done without PWM switching, which yielded power losses of 0.765W at 48V supply without PWM switching. Then incremental increase of the power consumption starting from 8kHz to 80kHz PWM was printed against the simulated COSS power losses. In addition, the phase voltage resistor divider losses for sensing the three phase voltages (when switching) were subtracted from the measurement too, in order not to add these to the COSS power losses. The simulation is a good match with the measured COSS power losses.