TIDUF68 February 2024
The efficiency testing was done at 27°C lab temperature using a HIOKI PW6001 Power Analyzer and HIOKI CT6872 current transformer. The TIDA-010936 was powered with 48V DC and a high-power servo motor was used as load (72V, 21A). A dynamometer supplies high load in the motor. The PWM carrier frequency was set from 40Hz to 80kHz. The motor speed is 600RPM. Figure 4-20 shows a picture of the test setup and block diagram for wiring.
For all of these tests neither a heat sink nor a fan were used, hence only natural convection of the TIDA-010936 PCB applied.
Figure 4-22 shows the TIDA-010936 power losses versus the three-phase motor load current in ARMS. These numbers do not include the power losses of the C2000 MCU LaunchPad development kit.
The TIDA-010936 board power losses at maximum load current of 14.8ARMS were 9.66W at 40kHz PWM and 10.5W 80kHz PWM. The TIDA-010936 power losses are dominated by the losses in the GaN FETs (LMG2100) and the losses in the 1mΩ shunt resistors.
The theoretical maximum peak efficiency at 48VDC with a maximum phase-to-phase voltage of 19.5VRMS (Space Vector PWM with 3rd harmonics) and a power factor of 0.9 is 99.3% at 40kHz PWM and 99.2% at 80kHz PWM, as shown in Figure 4-23.
Observe that while the PWM switching frequency increases, the power losses of the board do not increase significantly. This also reflects the very low switching losses of the LMG2100R044 GaN-FETs to help to achieve very high efficiency even at higher PWM switching frequencies.