TIDUF71 March 2024
The config file also has RXA and RXB channels configured with the NCO set to 2.1GHz. Inject a tone at 2140MHz. For proper SNR performance, the signal must be filtered. Adjust the amplitude of the fundamental signal to read approximately -3dBFS. This is likely a signal generator power around -10 to -12dBm.
Figure 3-5 shows the FFT spectrum from the single tone capture. SNR performance is around 51dBFS. SFDR performance is around 66dBFS. HD2,HD3 performance is very good at less than 85dBFS. Note, TXA and TXB are disengaged to eliminate any bleed-through component impacting the FFT capture.