TIDUF71 March 2024
The config file sets FB2 channel NCO to 1.7GHz. Inject a tone at 1740MHz through an appropriate band pass filter. For capturing the feedback channel, change the HSDC pro ini file to: AFE79xx_1x2FB_44210. Change the ADC data rate to 491.52M.
Adjust the amplitude of the fundamental signal to read approximately -3dBFS. This is likely a signal generator power around -10 to -14dBm depending on cable and filter loss.
Figure 3-7 shows the FFT spectrum from the single tone capture. SNR performance is around 43dBFS. All TX outputs are disengaged to maintain that FB spectrum is not contaminated.