TIDUF73 September 2024
The precharge design process begins with the requirements as the requirements are the most consequential aspect in the choice of components. Table 2-1 lists the requirements.
REQUIREMENT NAME | VALUE |
---|---|
Precharge Time | 0.5 seconds |
System Voltage | 800V (1000V) |
DC-Link Capacitance | 2mF |
This design must charge a 2mF DC-Link capacitor up to the system voltage of 800V in 0.5 seconds. However, 800V EVs can carry as much as 1000V at full charge, so the components in the design must be sized accordingly.