TIDUF77 June 2024 – December 2024 MSPM0G1507
Figure 2-21 shows the conventional PLL integrated into the SMO.
The traditional reduced-order sliding-mode observer is constructed, with the mathematical model shown in Equation 21 and the block diagram shown in Figure 2-22.
where
where
If kα and kβ are positive and significant enough to provide the stable operation of the SMO, then kα and kβ are large enough to hold
and
The estimated value of EEMF in α-β axes (Equation 25, Equation 26) can be obtained by low-pass filter from the discontinuous switching signals zα and zα:
where
is the cutoff angular frequency of the LPF, which is usually selected according to the fundamental frequency of the stator current
Therefore, the rotor position can be directly calculated from arc-tangent the back EMF, as Equation 29 defines:
Low-pass filters remove the high-frequency term of the sliding-mode function, which results in phase delay. The delay can be compensated by the relationship between the cut-off frequency ωc and back EMF frequency ωe, which is defined as shown in Equation 30:
Then the estimated rotor position by using SMO method is found with Equation 31:
In a digital control application, a time-discrete equation of the SMO is needed. The Euler method is the appropriate way to transform to a time-discrete observer. The time-discrete system matrix of Equation 21 in α-β coordinates is given by Equation 32 as:
where
The time-discrete form of Equation 27 is given by Equation 35 as: