TIDUF77 June 2024 – December 2024 MSPM0G1507
Permanent magnet synchronous motor (PMSM) is widely used in home appliance applications due to the high power density, high efficiency, and wide speed range. The PMSM includes two major types: the surface-mounted PMSM (SPM), and the interior PMSM (IPM). SPM motors are easier to control due to the linear relationship between the torque and q-axis current. However, the IPMSM has electromagnetic and reluctance torques due to a large saliency ratio. The total torque is non-linear with respect to the rotor angle. As a result, the MTPA technique can be used for IPM motors to optimize torque generation in the constant torque region. The aim of the field-weakening control is to optimize to reach the highest power and efficiency of a PMSM drive. Field-weakening control can enable a motor operation over the base speed, expanding the operating limits to reach speeds higher than rated speed and allow exceptional control across the entire speed and voltage range.
The voltage equations of the mathematical model of an IPMSM can be described in d-q coordinates as shown in Equation 45 and Equation 46.
Figure 2-25 shows the dynamic equivalent circuit of an IPM synchronous motor.
The total electromagnetic torque generated by the IPMSM can be expressed as Equation 47 that the produced torque is composed of two distinct terms. The first term corresponds to the mutual reaction torque occurring between torque current iq and the permanent magnet ψm, while the second term corresponds to the reluctance torque due to the differences in d-axis and q-axis inductance.
In most applications, IPMSM drives have speed and torque constraints, mainly due to inverter or motor rating currents and available DC link voltage limitations respectively. These constraints can be expressed with the mathematical equations Equation 48 and Equation 49.
where Vmax and Imaxare the maximum allowable voltage and current of the inverter or motor.
In a two-level three-phase Voltage Source Inverter (VSI) fed machine, the maximum achievable phase voltage is limited by the DC link voltage and the PWM strategy. The maximum voltage is limited to the value as shown in Equation 50 if Space Vector Modulation (SVPWM) is adopted.
Usually the stator resistance Rs is negligible at high speed operation and the derivative of the currents is zero in steady state, thus Equation 51 is obtained as shown.
The current limitation of Equation 48 produces a circle of radius Imax in the d-q plane, and the voltage limitation of Equation 50 produces an ellipse whose radius Vmax decreases as speed increases. The resultant d-q plane current vector must be controlled to obey the current and voltage constraints simultaneously. According to these constraints, three operation regions for the IPMSM can be distinguished as shown in Figure 2-26.
In the constant torque region, according to Equation 47, the total torque of an IPMSM includes the electromagnetic torque from the magnet flux linkage and the reluctance torque from the saliency between Ld and Lq. The electromagnetic torque is proportional to the q-axis current iq, and the reluctance torque is proportional to the multiplication of the d-axis current id, the q-axis current iq, and the difference between Ld and Lq.
Conventional vector control systems of SPM motors only utilizes electromagnetic torque by setting the commanded id to zero for non-field-weakening modes. But while the IPMSM utilizes the reluctance torque of the motor, the designer must also control the d-axis current. The aim of the MTPA control is to calculate the reference currents id and iq to maximize the ratio between produced electromagnetic torque and reluctance torque. The relationship between id and iq, and the vectorial sum of the stator current Is is shown in the following equations.
where
Equation 47 can be expressed as Equation 55 where Is substituted for id and iq.
Equation 55 shows that motor torque depends on the angle of the stator current vector:
This equation shows the maximum efficiency point can be calculated when the motor torque differential is equal to zero. The MTPA point can be found when this differential, Equation 56 is zero as given in Equation 57.
Following this equation, the current angle of the MTPA control can be derived as in Equation 58.
Thus, the effective d-axis and q-axis reference currents can be expressed by Equation 59 and Equation 60 using the current angle of the MTPA control.
However, as shown in Equation 58, the angle of the MTPA control, βmtpa is related to d-axis and q-axis inductance. This means that the variation of inductance impedes the ability to find the exceptional MTPA point. To improve the efficiency of a motor drive, estimate the d-axis and q-axis inductance online, but the parameters Ld and Lq are not easily measured online and are influenced by saturation effects. A robust Look-Up Table (LUT) method provides controllability under electrical parameter variations. Usually, to simplify the mathematical model, the coupling effect between d-axis and q-axis inductance can be neglected. Thus, assume that Ld changes with id only, and Lq changes with iq only. Consequently, d- and q-axis inductance can be modeled as a function of the d-q currents respectively, as shown in Equation 61 and Equation 62.
Reduce the ISR calculation burden by simplifying Equation 58. The motor-parameter-based constant, Kmtpa is expressed instead as Equation 64, where Kmtpa is computed in the background loop using the updated Ld and Lq.
A second intermediate variable, Gmtpa described in Equation 65, is defined to further simplify the calculation. Using Gmtpa, the angle of the MTPA control, βmtpa can be calculated as Equation 66. These two calculations are performed in the ISR to achieve a real current angle βmtpa.
In all cases, the magnetic flux can be weakened to extend the achievable speed range by acting on the direct axis current id. As a consequence of entering this constant power operating region, field-weakening control is chosen instead of the MTPA control used in constant power and voltage regions. Since the maximum inverter voltage is limited, PMSM motors cannot operate in such speed regions where the back-electromotive force, almost proportional to the permanent magnet field and motor speed, is higher than the maximum output voltage of the inverter. The direct control of magnet flux is not an option in PM motors. However, the air gap flux can be weakened by the demagnetizing effect due to the d-axis armature reaction by adding a negative id. Considering the voltage and current constraints, the armature current and the terminal voltage are limited as Equation 48 and Equation 49. The inverter input voltage (DC-Link voltage) variation limits the maximum output of the motor. Furthermore, the maximum fundamental motor voltage also depends on the PWM method used. In Equation 51, the IPMSM has two factors: one is a permanent magnet value and the other is made by inductance and current of flux.
Figure 2-27 shows the typical control structure is used to implement field weakening. βfw is the output of the field-weakening (FW) PI controller and generates the reference id and iq. Before the voltage magnitude reaches the limit, the input of the PI controller of FW is always positive and therefore the output is always saturated at 0.
Figure 2-16 and Figure 2-18 show the implementation of FAST or eSMO based FOC block diagram. The block diagrams provide an overview of the functions and variables of the FOC system. There are two control modules in the motor drive FOC system: one is MTPA control and the other one is field-weakening control. These two modules generate current angle βmtpa and βfw, respectively, based on input parameters as shown in Figure 2-28.
The switching control module is used to determine angle of application, and then calculate the reference id and iq as shown in Equation 53 and Equation 54. The current angle is chosen as in the following: Equation 67 and Equation 68.
The flow chart in Figure 2-29 shows the steps required to run InstaSPIN™-FOC with FW and MPTA in the main loop and interrupt.