TIDUF77 June 2024 – December 2024 MSPM0G1507
<install_location>\solutions\tida_010273_GaNInv
\f280013x\ccs\motor_control
Import the project within CCS and select the right build configurations by right-clicking on project name as shown in Figure 3-18. Select the right build configuration for the HVAC reference design. The Flash_MtrInv_3SC build configuration supports the three-shunt current sensing method, Flash_MtrInv_1SC supports the single-shunt current sensing method.
Configure the project
to select the supporting functions in the project by clicking Project →
Import CCS Projects, and browse to
<install_location>\solutions\
for F280013x based reference design, and then right-click on the imported project
name, click Properties command to set the pre-define symbols for the project
as shown in Figure 3-19.tida_010273_GaNInv
\f280013x\ccs\motor_control