TIDUF87 November 2024
A bidirectional power stage is used to charge and discharge batteries. In a normal start-up condition, buck converter output increases from 0V to the target voltage. If a battery load is connected while buck is ramping from 0V, this can result in large current overshoot. This problem can be avoided in two ways. The first method is starting the buck converter with output relay open, and setting the relay to closed position when buck converter reaches close to the battery voltage, as shown in the Figure 2-3. The second method is starting the buck converter in DCM mode with the low-side switch OFF during charging, or with the high-side OFF during discharging, as shown in Figure 2-4. A timer is required to switch from non-synchronous mode to synchronous mode.