TIDUF89 September 2024
The same SNR compensation technique to increase detection range over range and angle also serves to reject false alarms near the radar due to trees and bushes. Trees and bushes can be a persistent source of noise, especially in the areas where surveillance devices are installed. Assuming that stationary objects are rejected from the radar returns using the static clutter removal option, the RCS of trees and bushes, is often much smaller than that of a person. Therefore, at a given distance from the radar, points from a person walking and a tree blowing in the wind can be separated by SNR, (provided that the power degradation over range is accounted for).