TIDUF98A October 2024 – February 2025
The MSPM0L2228 has two SPI bus, one is connected to an external Serial FLASH device for logging data, while the other one is used to communicate with the ADS131M03 device.
The clock frequency for both is set to 8MHz in the TIDA_010940.syscfg file.