AC voltages and currents can be
applied to the board for testing purposes at these points:
- Terminal block J2 is a two-position
terminal block for the line and neutral voltage connections of ±270V
- Terminal block J14 is connected to the output terminals of the shunt. This
terminal block is also a two-position terminal block. For the gain of 32 used in
this design, the differential voltage across the two J14 terminals need to be
less than ±37.5mV.
Note: Phase A voltage has to be supplied to J2, Pin 1, which is
marked with DGND on the silkscreen, while Neutral is connected to J2, Pin 2.