TIDUF98 October 2024
Figure 2-1 depicts a high-level block diagram of this one-phase electricity meter application.
The resistance of the shunt current sensor is selected based on the maximum current value required for energy measurements and needs to also minimize the power dissipation of the shunt.
The choice of voltage divider resistors for the voltage channel is selected to make sure the Mains voltage is divided down to adhere to the normal input ranges of the ADS131M03 device. Since the ADS131M03 ADC have a large dynamic range and a large dynamic range is not needed to measure voltage, the voltage front-end circuitry is purposely selected so that the maximum voltage seen at the inputs of the voltage channel ADC is only a fraction of the full-scale voltage. By reducing the input voltage range, voltage-to-current crosstalk, which actually affects metrology accuracy more than voltage ADC accuracy, is reduced at the cost of voltage accuracy. In Figure 2-1, a simple voltage divider is used for translating the Mains voltage to a voltage that can be sensed by the ADC, while current sensor is used for sensing the line current, whereas the neutral current is not monitored.
In this design, only two ADC channels are used, hence using the pin-compatible ADS131M02 can reduce the system design cost even further. The ADS131M03 device interacts with the MCU in the following manner:
Other signals of interest in Figure 2-1 are the active and reactive energy pulses used for accuracy measurement and calibration, named ACT and REACT. The design supports an isolated RS-485 interface through the use of the ISO6731 and THVD1400 devices on the board.