The reference design uses a 4-layer
stack-up for the PCB. The stack-up is extremely critical for antenna performance.
This section elaborates on the existing stack up and a couple of layout related cost
reduction techniques implied.
Figure 3-22 shows the stack-up details of the PCB.
The antenna resides on the top layer
(Lyr 1) of the PCB. This layer has FR408HR dielectric material. Below are a few
critical properties of the dielectric:
- The dielectric has 2 x 1067 (dual
ply) spread glass construction. This structure helps reducing the glass weave
effect that helps reducing losses.
- Thickness of the dielectric is
5mils (127um). This thickness value is adjusted for impedance matching.
- The Dk value of the dielectric is
3.3
- This is core material.
Note: - The dielectric thickness must not be altered as this can cause impedance
mismatch and more reflection of the radiated power.
- Pre-preg material must not be
used for the antenna layer. For the layers in between other than antenna,
pre-preg can be used.
Grounded coplanar waveguide (GCPW)
transmission lines have been used to carry the RF signals to the antenna. Below are
some critical considerations for the antenna layer and the ground layer followed by
the same:
- Finished copper thickness on the
antenna layer is 40um.
- Ground plane (below the antenna
plane, Layer 2) thickness is 1oz (0.5oz can also be used if 1oz is not
available).
- PCB surface finish is OSP or
immersion silver.
Note: ENIG surface finish is NOT
recommended as this can potentially cause higher insertion losses for the
mmWave frequency range.
The overall PCB thickness of the
reference design is 1.6mm.
Note: We recommend using the TI stack-up as is. If a different
stack-up is desired, 3D EM solvers are recommended and antenna optimization needs to
be done.
Following are some of the techniques
implied to reduce the cost of PCB design: