TIDUFA8 November 2024
When low power mode is disabled (lowPowerCfg 0), the APLL supply stays at 1.4V always.
The APLL supply in low power mode (lowPowerCfg 1), stays at 1.4V initially, after the device power up and before configuration is sent. Once the configuration is sent the device starts chirping. During the active burst time of every frame the APLL supply rises sharply to and remains at 1.4V until the end of the active burst time. At the end of the active burst time, the supply drops to 0V until the next frame starts. Figure 2-11 and Figure 2-12 show the behavior of the 1.4V APLL supply, when the low power mode is enabled.
In low power operation the 1.4V APLL supply stays at 1.4V for a duration little longer than the active chirping duration, 5.4ms for this case, as the APLL needs to be turned off after the SYNTHESIZER turns off at the end of active chirping time. After that the supply drops to 0V until the next frame starts.