TIDUFA8 November 2024
On-chip LDOs require external capacitors for dominant pole compensation. For this, the capacitor placement and the output path traces become PCB design constraint dependent. The parasitic components contributed by the output path play a vital role in determining the system stability. In the previous section we have listed specific parasitic inductance and resistance values for each of the high bandwidth sensitive LDOs to make sure the stability of the power supplies. Here we are going to observe an example of good and bad practices while designing the PCB layout.
Figure 3-29 shows a design where the decap is placed far from the respective LDO-output BGA-balls. Considering the length of the complete trace connecting the balls to the capacitor lead by adding:
Figure 3-30 shows a design where the capacitor is places very close to the BGA balls. Considering the possibilities of system instability involved with the previous example, this design is much better as the parasitic values are within the data sheet spec.